Hi,
We have the following setup:
The drv8301 board with f2802 piccolo control card and the blackhawk xds100v2 ARM controller.
We are trying to configure via the code composer and getting the following error message while testing conncection:
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-151' (0xffffff69).
The title is 'SC_ERR_POD_OPEN'.
The explanation is:
This utility failed to open the adapter for a custom emulator.
The adapter returned an error.
[End]
the DRV8301 is powered.
ii'll note that the XDS is installed and connected properly, and used this exact board with INSTASPIN BLDC cc2803x control card and it worked fine.
any ideas as to what can be the problem?
p.s.
seems like my 14-pin JTAG connector is missing a pin. should it be like that or is it broken?
regards,
Nadav