Hello,
I am prepearing to design a system which will have 3 axis. I will use 3 PMSM motor in this design and system will do high precision positioning thats why i also use encoders and hall sensors. I searched and found your InstaSPIN-Motion solution.
But i want to learn something else if you can please help me:
1_There will be 3 independent motor drivers and 1 control unit in my design. Can i use your ınstaspin solution in order to generate interpolation in 3 axis?(i saw that we can do generate interpolation in 2 axis with one microcontroller)
2_Can i use analog positioning sensors with instaspin-motion?
For speed and resolution questions below i will use 3 phases and 4 pole pair or 1 pole pair PMSM motor with enough torque.
3_With a perfect mechanical design can i get 0.02 arcsec resolution with instaspin with encoder? I need high resolutions that is wy i asked for analog sensors.
4_With that maximum resolution and instaspin-motion ( i saw that supported microcontroller has 90 MHz clock speed) and without interpolation while positioning what rpm speed can i reach?
Thank You.