Hi,
I would like to know if there is any data(approx) about the device's
Junction Temperature(Tj) when it is operating at Maximum Frequency.
I tried to calculate it through Thermal Model info & Current Consumption info
from TMS320F28069' datasheet.
From the document "SPRA953B" Tjunction= Tambient+(θja x Power).
Tambient = 25°C (approx)
θja = 42.2°C/W (from datasheet Thermal Characteristics Table 5.8)
Power = 3.3V x 307mA (Maximum current consumption from datasheet Table 5.11)
So Tj=25°C + (42.2°C * 1) = 67°C (approx).
With the above calculation the Junction temperature(Tj) at Max Frequency(90Mhz)
would be around 67°C.
Please let me know if the above calculation is proper?
Regards
Kummi