Hi!
I use TMS320F28335, CCS5.2.
I have a question about DMA and ADC usage.
I want to use DMA move data of ADC to the buffer.
ADC: 16ch x 16 bit,
want to move data length: 256 x 16 bit.
DMA config:
// Set up SOURCE address:
DmaRegs.CH3.SRC_ADDR_SHADOW = (Uint32) &AdcMirror.ADCRESULT0;// Point to first RESULT reg
// Set up DESTINATION address:
DmaRegs.CH3.DST_ADDR_SHADOW = (Uint32) &ADCbuffer[0]; // Point to beginning of ADCbuffer
If can I get the 256 data with once interrupt of DMA?
What can I do?
please help!
Thanks!