Hello,
I hope someone can help me. I have the following problem:
I use CCS 6.1 and I want to run my application from flash.
With my Olimex XSD100v3 I am able to debug from ram as
well as from flash. Everything works fine.
The problem:
After restarting, the system doesn't run anymore. I have the
feelig that I do somethig wrong.
Do I have to consider something special if I write my application
to flash? Do I have to change something in the code?
Untill now I just changed the debug mode from ram to flash.
I am looking forward to your answers.
Greets.