Good Afternoon
I am working on windows 7, 64 bit.
using CCS v6.1
Variant : 2833xDelfino , TMS320F28335
Connection: XDS100v1 USB Emulator
Compiler Version TI v6.4.2
I am working on ADCs and i see a very weird problem.
Even if I do not give any input at ADC pins, still the pins are at some (0.6-1)V and it varies from pin to pin in this range.
Today i supplied my ADCIN0 with a simple potential divider circuit with 0.5 V. (Input to potential divider circuit was given from a regulated power supply at 5 V)
Before giving external supply to adc pin, it was at 0.6 V. But after I supplied the pin from my potentiometer it showed voltage of 1.6V
I checked all my groundings thoroughly.
But, I am not able to understand that why ADC pins are at some voltage already.
And how can I overcome from this problem?
With Regards