Hello,
I was wondering what the licensing was for various source files in controlsuite.
I"ve seen https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/342911 and essentially we have the exact opposite concern. Namely, we have a piece of software we want to open source and make available that has dependencies on the binary flash libraries as well as some of the driverlib components. Ideally we want to just check these files in so that it is easier for people to use, and so that we keep fine grain control over which version of these things the various components use.
This is pretty much how we do it in our private repo so that developers can easily build without having to download or configure the whole of controlsuite if they aren't mainly working on the DSP portion of our project, and it works well. The alternative would be to re-do our project links to use the CCS_INSTALL_ROOT variable in eclipse, and provide instructions on how and where to download the controlsuite. Not insurmountable, but annoying to people wanting to look at the project.
Have a good one!