I have a project running on the DSP which uses the MiniUSB of the controlCARD. I could connect it to a Win7 Laptop, which successfully recognizes the USB bulk device (after installing the Windows driver from the control suite). Now I would like to do the same with a Win10 Laptop, but when trying to install the Windows driver from the TI control suite i get an error message.
A rough translation of the german error message: The hash value of the file is not in the catalog file. Probably the file has been damaged or changed without permission.
Is this a driver compatibility problem with Win 10?