Hi,
I developed a program and tested with eZDSP28335 kit which worked as expected, later a custom board with TMS320F28335 was designed, the same program was loaded but after few seconds it is going to illegal isr (or any one of the trap) I couldn't figure out the reason. Do any one have any idea what could be the reason?
In project properties I changed the device information when changing the board other than that no change was made.
XDS100V2 emulater used in both the cases.
I tested some of the example program available from control suite, the response is same the program is working fine in eZDSP kit but going to illegal isr (or any one of the trap) in the custom board.