I found numerous references to the blank micro problem on the web. Apparently the early release circa 2010 was shipped without code installed. The GUI application wasn't on the thumb drive either. No matter, I downloaded the GUI and also "How to: FLash the DC/DC LED Lighting Kit's F28035 controlCARD so that it works with the GUI" and followed the procedure. First, the code wouldn't compile, casting numerous errors about various #include paths not including the "Dir". I tried to sort this out from the makefile, but couldn't find any problem with it. The files were wher the include path directives said they should be. I had been trying to rebuild the project with CCS5.5.0, so I installed CCS v4 from the CD include with the kit and tried again. Same result. So... I found an already compiled .out file and tried to load it directly from the CCS debugger as recommended in the "How To". Now, the Connect Target command failed with the following error: Error connecting to the target: Error 0x00001200/-1135 Error during: OCS, Target, Unrecoverable emulation error. Which indicates that CCS is not communicating with the USB/JTAG emulator - which is on board the kit pcb - properly. I verified all jumpers, power supplies and cable connections to no avail. What I would like to do is return this unit to the distributor and get a new one from TI direct - presumably with the code in the micro this time, such that I can run the GUI without writing an entire new project. The distributor says they will not accept a return until TI support has agreed that there is a problem.
Please help me resolve this so I can continue my evaluation of this device.
thank you,
Robert E. Stephens
Physical Optics Corporation