Hi,
I checked connection of HVPSFB and GUI (PCMC) and test.
It can monitor data of HVPSFB Kit.
1. J1 is populated and R6 is opened on control card.
2. Apply an appropriate resistive load to the PSFB system at the DC output.
3. First I connect USB connector to the Piccolo control card for emulation.
4. Power the input at J1, J2 with 400V DC. No external bias supply.
5. I build and load project in CCS.
6. And then run the code by using the <F8> Key.
But program don't run and error message is occurred.
Error 1
C28xx: Error: (Error -1041 @ 0xFFFFFF6A) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.1.507.0)
C28xx: Trouble Halting Target CPU: (Error -150 @ 0x0) One of the FTDI driver functions used during configuration returned a invalid status or an error. (Emulation package 5.1.507.0)
C28xx: Unable to determine target status after 20 attempts
C28xx: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
Error 2
C28xx: Error: (Error -150 @ 0x0) One of the FTDI driver functions used during configuration returned a invalid status or an error. (Emulation package 5.1.507.0)
C28xx: Unable to determine target status after 20 attempts
C28xx: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging.
I want test and road modified source in CCS.
Did I miss something?