Hi,
I am trying to make PSFB configuration with F28377S. Is it possible to make high resolution period and high resolution phase control at the same time with fixed dead time with F28377S?
Refering TRM chapter 14.1
• Enables high resolution output swapping on the EPWMxA and EPWMxB output
• Enables high-resolution output on EPWMxB signal output via inversion of EPWMxA signal output
Does these mean that, EPWMxB is an inversion of EPWMxA for F28377S, and there is no dead band support for EPWMxB? because next line is a bit confusing
• Enables high-resolution period, duty and phase control on the EPWMxA and EPWMxB output on
devices with an ePWM module.
Or this mean that EPWMxB is not just an inversion of EPWMxA, and EPWMxB has dead band support?
Is there any sample code?
What i found from controlsuite is,
C:\ti\controlSUITE\device_support\F2837xS\v170\F2837xS_examples_Cpu1\hrpwm_prdupdown_sfo_v8
for high resolution period control.
Or can i think this as a starting point
C:\ti\controlSUITE\libs\app_libs\digital_power\f28x7x_v1.0\CNF\PWM_1chHiRes_Cnf.c
is there any where else that i should check?
Thank you for your help