Hi,
From Technical reference manual, it seems like dsp F28377D does not provide a register shared between cpu1 and cpu2 with atomic operations, is this correct?
if yes, Please, do you plan do add this?
Thanks,
Regards,
Rony.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
From Technical reference manual, it seems like dsp F28377D does not provide a register shared between cpu1 and cpu2 with atomic operations, is this correct?
if yes, Please, do you plan do add this?
Thanks,
Regards,
Rony.
Hi Rony,
That is correct. There is a register-based mechanism for data exchange between CPUs (IPC), but I doubt this is what you meant.
F28x7x parts are in full production. There are no plans to add a feature like this.
Regards,
Richard
Hi Rony,
It'll be good if you could give example of shared resource or register in this case? Most of the shared resources are allocated to CPU1 or CPU2 as part of system initialization hence need not to have IPC handshake during application run time. Some registers are semaphore based and there an IPC handshake may be needed but most of these are related to clock configuration which are also done as part of system initialization. So it really depends on which shared resource/register we are discussing here and what is the use case.
Regards,
Vivek Singh