Hi,
Does anyone have open loop bode plot of HV_DC_AC inverter? I cannot find it in the user manual. I'm trying to use another controller (PI OR PR). So if you have any reference about this, please let me know. Thanks!
I've used powersuite to plot the open loop bode diagram of single phase DC-AC inverter. I put the same parameter in it, but the plot is different from the one I plot using Matlab. See the red line in Fig.1 and blue line in Fig.2. That's the transfer function without current controller. The crossover frequency and phase angle are different.
fig.1
fig.2
BR,
Jiao Jiao