Hi,
I'm trying to use the serial_programmer. I'm using Controlsuit version v3.4.0 - June 27, 2016.
files for 28027 - V230.
I'm able to download the kernel, but after that the programmer hangs.
Looking at the implementation of the PC side, (C:\ti\controlSUITE\device_support\~Utilities\serial_flash_programmer), I see major differences compared to the 28027 side:
1. 28027 waits for:
if (SCIA_GetOnlyWordData() != 0x08AA) return FLASH_ENTRY_POINT;
ReadReservedFn();
which the PC-side does not support.
2. 28027 does not send back ACK.
and so on...
Is this solution verified to work?
Further, something I noticed in the cmd file of the kernel:
BOOTROM : origin = 0x3FF27C, length = 0x000D44
According to SPRUFN6A, the bootrom are in 0x3FF4B0.
Thanks a lot