I have a very similar problem as discussed in https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/394313 , and https://e2e.ti.com/support/microcontrollers/c2000/int-c2000/f/175/t/519686 . On a failed device, the 3.3V rail reads ~20-ohms, the 1.9V rail ~4-ohms.
The power sequence of 3.3V ramping first, followed by 1.9V only after the 3.3V rail is > 2.5V is being adhered to, so I don't believe the ON sequencing is an issue. But what about power-OFF sequence?
Also, as previous post pointed out, having a voltage present on an IO or ADC pin, and no current-limit protection, is described in the 'F28335, but I don't see it discussed in the 'F2812 datasheet. Does the same condition also apply for this processor?
I'm not sure what additional information will assist with troubleshooting this failure. What other info might you need to help determine the cause of failure?
In addition to the low resistance on these power rails, when power is applied to a failing device, the F2812 is constantly RESETing at about a 250Ha rate. It is also outputting a CLK of about 4MHz.
~Leonard