Hi everybody,
I have been using asm2000 to generate .obj and .lst file. Ever since I have moved to windows 10, .obj file is not generated, but .lst is generated normally without any assembler errors or warnings. I have also tried disabling the antivirus. Tried using cl2000 as mentioned in other threads, but .obj file that it outputs is significantly different from the ones I used to get on win 7. Also the .lst file is not generated while using cl2000 :( Does anyone have any guesses?
command line looks like this:
asm2000.exe -i".\inclusion_folder1" -i"inclusion_folder2" -ad=_FLAG1=0 -ad=_FLAG2=0 -ad=_CPUCLK=150 -d"LARGE_MODEL" -mf -v28 --float_support=fpu32 -m20 -l -s "SOURCE.ASM" DEST.OBJ DEST.LST
invocation of cl2000 looks like this:
cl2000.exe -i"inclusion_folder1" -i"inclusion_folder2" -ad=_FLAG1=0 -ad=_FLAG2=0 -ad=_CPUCLK=150 -ml -v28 --float_support=fpu32 -m20 -s "SOURCE.ASM" DEST.OBJ DEST.LST
Thanks for the help and kind regards,
Nikola