If I assign ownership of the ADCs to CPU2, it states that the data registers are still readable by all processors, so if CLA on CPU2 is reading the ADC, which bus is it using?
If CPU2 is reading a ADC register and the CLA on CPU2 is reading a register, are they using the same bus? or
The documentation talks about the CLA bus in the context of accessing shared memory, but doesn't really state with regard to say the ADC registers.
Does the CLA use the CLA bus to access the ADC data registers, just like memory, so there is no conflict with the CPU running it's programs and/or reading the ADC registers?