Dear all,
I have problems to run correctly the lab4 (torque control) when a load is fixed to the axle of the motor.
I have run lab2a, lab3a, lab3b and lab4 using a PMSM motor with no load. The labs has been executed without problems. (Lab4 has been modify in order to limit the speed and to receive iq references via CAN).
Then I have fixed (using a flexible copling) a load to this motor. The load is basically an asynchronous motor with a speed control and a reference speed fixed to 0 rpm. The torque used by this control is modified by CAN and it is used as a resistive torque for the PMSM controlled with instaspin.
If the resistive torque (TL) applied to the PMSM is fixed to 0Nm then the lab4 works OK. Once the cogging torque and static torque is overtaken the motor accelerates (depending on the iq reference). Once the motor is spinning the load (resistive torque) can be increased without any problem.
Now, if we try to start the motor with a load fixed to the axle (for instance 1Nm of resistive torque) the motor do not start spinning or a huge current is needed to start it. The controls moves the motor roughly (start, stop, start, stop and so on) during some seconds and then (sometimes) the motors start to spin softly.
It seems like the controls has problem to identify the motor position. In fact, I have repeated lab3b and I have seen that the motor is moving roughly with speeds below 300rpm (5% Rated Speed). When no load is present the motor has a huge acceleration and this speed (300rpm) is achived easily with small Iq references. When a load is fixed to the motor the motor the acceleration rate is limited and it probably has problem to identify the position. Could it be posible?
My application implies a heavy loads and the motor itself has a quite big cogging torque (10s to achive rated speed). Having this in count is it possible to have a soft start with sensorless methods or is it an unrealistic target?
Thank you in advance