Hi,
I have a lot of small questions on the Instaspin motion. I use a modified Lab13C
- How do I read the current the motor used. Or do I have to calculate them from Ibias.
- If I just want the motor to spin. in previous(intraspin FOC) examples you give a value to gMotorVars.SpeedRef_krpm. Is the a way to let the motor just spinning at a given RPM with intaspin motion?
- If I make a function: Start controller, wait controller to become ready, Motor do something. Nothing happens, because the main loop is never served. so can I make a Interrupt timer routine for this functions. How fast needs it to be serviced?
- does CPU_USAGE.h Also work with Instraspin motion? Is there any document on how to use it.
- Is it correct that no timers are used in Proj_Lab13C?
- where is mainISR attached to the interrupt controller?
Can you please add some variable description text in typedef struct _MOTOR_Vars_t_ It is a bit short.