Dear sir/madam,
In InstaSpin lab, the speed PID controller is in parallel form, while the current PID controller is in series form.
I don't know what cause them different.
Best regards,
Qian.Miao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear sir/madam,
In InstaSpin lab, the speed PID controller is in parallel form, while the current PID controller is in series form.
I don't know what cause them different.
Best regards,
Qian.Miao
Hi Qian.Miao,
This is a very good question, which I can only speculate as to why this occurred. It goes back to the legacy code from which InstaSPIN was derived.
As you know, both the series and the parallel form are identical from the perspective of a linear transfer function. I suspect that in the original code, they were both probably in parallel form. But then it was discovered that for the current PI controllers, the PI coefficient calculation is more straightforward if the structure is series rather than parallel. You can read more about this in my blog series on designing PI controllers: http://e2e.ti.com/blogs_/b/motordrivecontrol/archive/2013/02/28/teaching-your-pi-controller-to-behave-part-i
So I would guess that the current PI controllers were converted to series form to accommodate the self-tuning algorithm, but they didn't bother to also change the speed PI regulator since the same tuning advantage doesn't exist for the speed loop.
That's my best guess...
Regards,
Dave