I have designed an Inverter to attach to the Launchpad that is modeled after the BOOTXL. However this inverter does not use the DRV8301 but rather three 8 pin gate drivers. I have also updated user.h for this new inverter and removed the #define drv8301_spi
Using Lab2b, I am able to identify the motor and the motor spins good. The main problem is that the MOSFETS and gate drivers get very hot with no motor load! Running the same motor, the BOOSTXL board only gets a little warm even under load. The inverter is drawing about 10 times more current than the BOOSTXL inverter board. Something is really wrong here. My MOSFETs have a little higher total gate charge. But I don't see that making this huge of a difference. Could it be a dead time problem? Below is the schematic of one phase of my inverter. Any ideas gents?