Hello community,
I have developped an own simple hardware to control a PMSM motor with a dc link of 300V and a power of 500W.
Voltage measurement is realized by simple voltage divider and 3-phase current measurements by shunts at low side FETs with
positive gain opamps.
Values at user.h have been adapted.
When I apply external voltage at the dc-link, phase u, v, w voltage dividers, or a DC current of 1A through the shunts,
the values in the software seem to be OK.
When I start running with disconnected motor, the drain source voltages look fine.
But when I start running or identifying with connected motor, there is a high current consumption, limitted by my DC power supply.
Is there a possibility to test my hardware by open loop control, so just controlling the bridge with a certain PWM and rotating frequency
in order to check, if my gate driver and MosFets work correctly.
Thank you and kind regards,
Joachim