Hello everybody,
I have two questions for my application Piccolo with DRV8305 Boosterpack:
1) a) Is it possible to have stable rotor rotation below 100rpm (12hz on the scope) with enough torque? Below 90rpm it is jerky and
tends to stall with no mechanical load. Max torque before stall on the GUI indication is 0.6Nm at 100rpm,with supply dc current=0.4A and Vdc=35V.
Some of the motor specs are listed below:
USER_MOTOR_TYPE MOTOR_Type_Pm
USER_MOTOR_NUM_POLE_PAIRS (7)
USER_MOTOR_Rs (0.01959898)
USER_MOTOR_Ls_d (0.00002308)
USER_MOTOR_RATED_FLUX (0.026944)
Nominal motor max Voltage 50V and max current 60A. I never use the motor under high load with DRV8305 boosterpack.
Take in mind that the Rs, Ls and Flux values are not necessarily absloluteley right, more likely they are
close to reality.
b) Is there any project for DRV8305 BOOSTERPACK, for zero speed start under load like HFI?
2) Can I change the rotation direction through the software (without changing the phase terminals connection)?
Which variable inside the code defines the rotation direction? I want to change the rotation from
clockwise to counter-clockwise in stand alone mode, using an external switch.
Is it feasible with the FAST observer or there are limitations?
Could you suggest me any document guides for these?
Thanks,
Leo