Greetings -
I have an IPM motor that identifies and runs OK on lab_2b on the LAUNCHXL-F28027F. I can start, stop, etc, but the phases are very non-sinusoidal, even at higher loads.
On attempting to run lab 3a, the motor has a very difficult time starting. It is jumping quite a bit. in many different directions, but will sometimes jump in the right direction and get started after a minute or two.
My motor parameters:
#define USER_MOTOR_TYPE MOTOR_Type_Pm
#define USER_MOTOR_NUM_POLE_PAIRS (2)
#define USER_MOTOR_Rr (0.0)
#define USER_MOTOR_Rs (0.02587504)
#define USER_MOTOR_Ls_d (3.05e-5)
#define USER_MOTOR_Ls_q (3.05e-5)
#define USER_MOTOR_RATED_FLUX (0.0)
#define USER_MOTOR_MAGNETIZING_CURRENT (0.0)
#define USER_MOTOR_RES_EST_CURRENT (1.0)
#define USER_MOTOR_IND_EST_CURRENT (-1.0)
#define USER_MOTOR_MAX_CURRENT (6.0)
#define USER_MOTOR_FLUX_EST_FREQ_Hz (150.0)
As this is an IPM motor, I was expecting that the Ld would be different from the Lq, but they are exactly the same. Thank you for your time,
j