Part Number: DRV8312-C2-KIT
Hello,
I'm working with the InstaSpin_BLDC example project for the DRV8312-C2-Kit. I have 3 issues I hope you can assist me with:
- I want to drive two identical sensorless 3-phase permanent-magnet motors in perfect synchronization, i.e. applying the same phase voltages to each phase between the two. I have tried to simply connect the phase output for one motor to both motors (so for the 3 output terminals I stuck in 6 cables in total [MOA goes to phase A1 of motor 1 and phase A2 of motor 2, and so on...]). But when I run the InstaSpin application, the execution crashes early on without spinning the motor (only jumping a few steps by the sound of it) and I need to reset the board. I'm no electrical engineer and have a hard time wrapping my head around these kinds of sensorless motor drivers. I'm not sure how to trouble-shoot this. Is my approach even possible for the InstaSpin driver?
- Driving a single motor with the InstaSpin application works fine. I want to read out the power usage of the motor (current draw, voltage), but I am unsure how to calculate those values from the data provided. All I can find is some oddly sized "per-unit" (?) values. Can someone tell me what values I need to transform in which way to receive motor voltage in Volt and current in Amps?
- Max. speed problem: when entering high speed values (>0.5), my motor can only ever accelerate to 0.42 speed (~1650 RPM) and holds stable there, even though it is rated for over 4400 RPM. What might be the limiting issue here?