I would like to create two separate projects in CCS 5/6 for TMS570LS3137.
1. Project 1 will have drivers, middleware and RTOS code,
2. Project 2 will have application code.
I would be generating two separate binaries for each project, which would be flashed in two different memory sections in flash.
Is there a method in CCS 5/6 to generate a Symbol definition file for Project 1, which I can provide as an input at linker stage of Project 2.
The reason for this would be that, I would not have have to share the complete source code or even binary project 1 for implementation of project 2.
when both binaries are flashed on target, they would be able find appropriate symbols.