I have downloaded and run the Red Hat MSP430 Linux development tools, msp430-gcc-full-linux-installer-4.0.1.0.run. The C compiler runs successfully when executed with the LEDBlink sample code. My problem comes when I try to run the gdb debugger to download the object file resulting from the compiler (msp430f2013.out). I have attached a screen capture of the result of starting the debugger. It appears that some Python libraries are missing. Is there a list of the dependencies required for mspgdb to run? ]