This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Stellaris Launchpad additional USB examples and labs (Includes gamepad and combination Keyboard+Mouse device)

For those of you attempting to build USB devices in CCS I put together some additional Launchpad examples as well as a lab type walkthrough of how to create custom devices using some shortcut code (mainly HID based). This includes combination HID devices which don't currently work using the composite code in the 9453 library.

 Included

1) Examples ported to the Launchpad  - Mouse, Keyboard, Composite (Hid+CDC)

2) Updated HID header file with additional device and usage types

3) A new device type called usbdhidcustom - This allows you to make new devices with minimal code changes

4) A complete document in lab type format where you build a volume control device, a gamepad and a keyboard + mouse based on usbdhidcustom

5) Completed projects to go with the labs (Volume Control, Gamepad, Keyboard + Mouse device).