This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 2
Views: 187
Part Number: DRV8825
Hi,
I have some questions about DRV8825.
On the customer’s application, STEP frequency is changed during operation.
The current is distorted while low STEP frequency, but no problem while high STEP frequency.
To improve above, the decay mode need to be changed between mixed and fast.
Following current waveform shows same STEP frequency(500Hz) and different decay mode.
To change decay mode from mixed to fast, the current distortion will be disappear.
<Question>
(1)Can I change decay mode between mixed and fast without RESET during operation?
(2) Can I change decay mode between mixed and fast with RESET during operation?
(3) Do you have suggested schematic for changing decay mode between mixed(DECAY=open) and fast(DECAY=high)?
Best regards,
Masumi Sekiguchi
James Lockridge
Motor Drives
Best Regards,
Wang Li
Motor Drive Solutions