Hi,
I open new thread, because the original thread is locked.
Could you check the logic using 1xPWM mode with DRV8323RH?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I open new thread, because the original thread is locked.
Could you check the logic using 1xPWM mode with DRV8323RH?
Adam,
I showed the scope images in the previous thread.
GHx, GLx signal was cheked. But it was different from truth table with 1xPWM mode.
Thank you.
Adam,
GHA is PWM, then GHB and GHC should be low.
But, GHC is high and GLC is low
you can see the scope iamges in the previous thread.
first scope image showed GHB and GLB when GHA was PWM.
GHB is low and GLB is high (<-- it means GHC and GLC should be low)
second scope image showed GHC and GLC when GHA was PWM.
GHC is high and GLC is low (<-- I think it is different from truth table.)
thank you.
Adam,
I use DRV8323RH(hardware-interface). I left the mode pins open.
I think motor wires and hall sensors are connected well. When I applied the power, motor rotates well.
But I wonder the gate signals.
thank you.
Min-su,
Your hall inputs are probably not aligned with your motor inputs.
Regards,
-Adam
Adam,
I'm sure that hall and motor input connection is correct.
You can see the movie clip using 1xPWM mode.
https://www.youtube.com/watch?v=EKlaZy3hWHQ
Thank you.
Adam,
You can see the MOT signal in the previous thread.
MOT C is always high.I think it means the FET is ON.
Regards,
Adam,
Yes, the motor phase wires were not connected.
When I connected the phase wire, motor worked well.
Unfortunately, the experiment setup was disassembed.
Could you check the gate and phase signal?
Thank you.