Other Parts Discussed in Thread: DRV8301, DRV832X
DRV8323, shunt amplifier, RC filter design
I’m trying to figure out how can I calculate the output RC circuit of Shunt amplifier / ADC frontend.
My settings are
- Gain=40
- Bidirectinoal 3phase current meaurements via 1mOhm shunt resisistance . Current +-37,5A -> +-20A work area
- Vref = 3V
- ADC input capacitance – 4pF – STM32H750.
- Tasq – 41ns
- ADC resolution 16bit . target ENOB 10..12bits
Available info from DRV8323 datasheet
Output current – 0..5mA – recommended condition
Gain 5,10,20,40
Slew Rate = 10V/usec @60pF load
Unity gain BW =1MHz
My question is how can I calculate the output RC filter from provided data?
- Know methoth requires to know , the sunt amplifier Pole or bode diagram. I don’t know the output impedance of amplifier too.
- E2e community searach points me to this thread, but it does not give solution too.
https://e2e.ti.com/support/motor-drivers/f/38/t/838906
Even more it becomes more confusing. It seems the R6 is datasheet does not exist. I knew that similar drawing is shown in DR8301 datasheet and R6=100Ohm
- Copy paste existing solution – TI evauation module TIDA uses 100Ohm and 3n3 , but this solution is coupled with MSP430
Up until now I found the following solution. Use TI TIDA values of 100ohm, 3n3 as reference. Via trial and error find the best value. I’m sure that this is not the right way.
Can you please provide me with solution , document reference etc.?
Thanks in advance
Mirtcho Maglijanov