Hi,
I set the driver as in the figure below.
I chosse a sense resistor 0R68 to achieve a chop current of 1A, according to the datasheet (page 20).
I'm using the part number ST4209X1004-A of Nanotec.
I have to main problems:
1) When the motor is enables, when no PWM is present I can read a sink current of 1A from my power supply. When a PWM is present I read a sink current of 200mA. I also see this behaviour with the voltge across the R_sense;
2) If I set a pwm frequency greater than 50kHz, the motor is vibrating without moving;
have I wrong something?
Thank you for your precious support.