Hello! I have posted some threads about sudden and strange faults while working with DRV8302, without finding out anything (thread's links are under the cut). I suppose one thing to be the reason of my problems with IC. I use DRV8302 to control Brushed DC motor, so i am using only A and B channels, all pins of channel C stay in air (input pins and output), is it normal or not, what ping of unused channel i NEED to pull down or pull up. Can it be the reason of random faults? Thanks!