Referring to the datasheet section 7.4, there is a note to hold STEP low while coming out of nSLEEP or when applying power. The question would be does STEP need to be held low while the device is in the SLEEP state, or can the device be powered up into SLEEP mode?
In this same section there is also a note that says tSLEEP must elapse after falling edge on the nSLEEP pin. This makes me think that holding the nSLEEP pin low during power up would not keep the device in sleep since it is waiting for a falling edge?
In my situation, STEP is tied to MCU so it can be held low for steady state, but the power on sequence might be unknown. Motor driver gets power from a source that is expected to reach steady state before MCU gets its power source, but otherwise the full board gets power at the same time.
1) Are there any problems with having activity on the STEP pin while the device is in SLEEP?
2) Can the device immediately go into SLEEP at power on, preventing any errors from having the STEP pin not being held low?