Other Parts Discussed in Thread: DRV10987,
Tool/software: WEBENCH® Design Tools
Hi,
We are working on a 36Watt BLDC motor based on DRV10987.
Specifications of Motor
Wattage: 36Watt,
RPM: 360
Number of Poles: 16
We are facing the below issues while doing the register configuration with DRV10987EVM.
1) Fan initially rotating at High speed for low-speed command.
If we give 10% motor speed through I2C command (51) the fan is initially rotating at very high speed and then within 4 to 5 seconds it reaching its original speed (10% - 51)
2) RPM is not showing correctly in DRV10987 GUI Display Tab
The actual RPM of the motor at 10% is 36. But in GUI it is showing 691.
3) Always getting BEMF abnormal error.
While doing simulation the GUI is showing always BEMF abnormal issue. But it is not getting clear when we change the BEMF values.
For reference, I am attaching the screenshots of the GUI. Please clarify the above points.
Thanks & Regards,