Hi
I'm setting up a circuit to drive a 220v AC solenoid valve driver using the DRV110EVM
I configure EVM in the following way
- 220V AC connected to P2.1 P2.4
- Solenoid rated 220v AC 3-6W ( 160ohm and 204mH) connected on P1.2 - P1.4
- JP1, JP2, JP4 closed all the other open
I set the PWM frequency around 20Khz
than i regulate the PEAK trimmer in the middle (1,41V Vpeak) and than I enable the DRV110
the solenoid valve toggle from closed (no power) to open in almost or range of the HOLD trimmer and the PWM duty cycle is very low and ranges from 5% to 7% turning the HOLD trimmer from max to min
Here a screenshot of the DRV 110 Vout signal and is the same for the various hold trimmer position
What is wrong in my setup?
How can I regulate the hold current / PWM duty cycle ?
sure of your support
br
Davide