Other Parts Discussed in Thread: DRV2700,
To drive a piezoelectric actuator, a output signal with higher frequency (75kHz ~ 120kHz) and high output voltage (80Vpp) are required. In datasheet for DRV8662 and DRV2700, the maximum frequency is 20kHz that less than 120kHz. Is there other IC can meet the driving signal for our piezoelectric actuator?
Thanks for all help!