Hi all,
I would like to use DRV2700EVM to move a Pizo plate. I am making a "tactile stimulator" device where subjects place their hands on the piezo and detect a brief tap on their finger. I have a LabJack device that can produce an analog output with the range of 0-5 V. I would like to feed this into the piezo driver and would like the driver to (just) amplify the analog input and drive the Pizeo with it. The input is going to be a single square pulse, the output does not need to be a square, I can live with some filtering if turning off the filter is too hard.
I tried to follow the instructions but have not been able to set the jumpers and settings in GUI to get this going. Any help would be very appreciated. Needless to say, I am not an engineer so bear with me :)
Thanks a lot,
AZ