Other Parts Discussed in Thread: DRV2700
Hi,
I'd like to use the DRV2700EVM-HV500 to switch a 14pF load between 0V and 400V, ideally at a frequency above 10kHz.
The DRV2700 datasheet reports a low-gain bandwidth of 20kHz, however, I understand the low-pass filter in the EVM limits the maximum frequency.
What's the maximum frequency I can switch this load at with the EVM?
Is it possible to modify the parameters of the filter to move the 3dB point upwards, or even bypass it?
Thanks.