Sir/Madam
After I am giving the power supply of +1.8V to 1.8V pin in EVM board, I checked the voltage level in banana cable connector pin at TX-SDK-V2 EVM board. It showed +1.4V only but as per datasheet of LM96570, the digital core voltage should be in the operating ratings between +1.71V to +1.89V. Will it (+1.4) affect the operation of lm96570 IC? also I am not getting the output.
Thanks,