Hi all,
I'm wondering if TI produces any HV window supervisory IC which I can use to monitor a battery voltage (that can go upto 30V MAX) in order to disable a P-Channel MOSFET when the battery voltage drops below level A and re-enable it when it comes back to level B (having level B > level A).
I looked at the TPS3701 but unfortunately it's output pin (which I would have connected to the pull-down resistor on the gate on the P-MOS) goes up to 25V MAX, but >25V will definitely appear on it.
Cheers!
Aleks