Hello,
We are using engineering model (TPS7H1101HKR/EM) of TPS7H1101A-SP SPACE GRADE LDO and will be going for assembly in one or two weeks.
The package of TPS7H1101HKR/EM is ceramic dual flat pack. The pins and bottom themal pad are not aligned and in order to make contact between pins and PCB, the pins need to be bend otherwise ,thermal pad in the bottom of IC will make contact with PCB and pins will be floating during reflow process.
Along with TPS7H1101HKR/EM, we are also using engineering model of SPACE GRADE components given below
Part Number |
Description |
LMX2615W-MPR |
Clock Synthesizer |
TMP461HKU/EM |
Temperature Sensor |
TPS50601HKH/EM |
DC-DC Switching Regulator |
TPS7H3301HKR/EM |
DDR Termination Regulator |
and all this components have ceramic flat pack same as that of TPS7H1101HKR/EM.
I have seen a video from Fancort Industries, and they are bending the pins using some machines.
Here is the link https://youtu.be/hwblw74KTUA .
So, I have following questions :
- Is there any method of bending pins manually without using machines so that they can make contact with board during assembly process?
- Which soldering process to be used- ROHS or NON-ROHS?
Infact will you guys,please fill the below parameters related to soldering process as I am not able to find these in datasheets:
Parameters |
TI's Response |
Soldering Process(ROHS or NON-ROHS) |
|
MSL Level |
|
Baking Time |
|
Baking Temperature |
|
Peak Soldering Temperature |
|
Minimum Preheat Temperature and time |
|
Maximum Preheat Temperature and time |
|
Ramp-Up Time |
|
Ramp-Down Time |
|
It will be better if you guys can share SOLDERING PROFILE GRAPH indicating all these parameters.
And I am guessing same soldering profile can be used with all the components listed above. Am I right about that?
An early response will be highly appreciated as we are planning for assembly in one or two weeks.
Thanks & Regards,
Lalit