Hi,
I am Looking for the best PMIC that will fit for my design. The requirements are given below:
- Input:
- 3.5V to 4.2V
- Typically 3.7V
- Output 1:
- Vout: 3.3V
- I out maximum: 0.4 A
- I out normal: 0.3 A
- Output 2:
- Vout: 1.5V
- I out maximum: 0.2 A
- I out normal: 0.15 A
- Output 3:
- Vout: 1.2V
- I out maximum: 0.5 A
- I out normal: 0.4 A
The PMIC should be as small as possible. Please help me to find the best PMIC for the above requirements.