Other Parts Discussed in Thread: TL431
Tool/software: WEBENCH设计工具
Hi!
I use LM5023 to develop a boost power supply, VCC auxiliary supply voltage is 24 V, power MOSFET voltage is 3 V. Request to raise 3V to 36V, there are problems in debugging, special help support, thank you!
The current problem is that the output voltage can only be adjusted to 13V can not be raised, transformer parameters for PQ2016, primary use 3TSs, auxiliary winding is 4TSs, output winding is 18TS.LP:2.8uH.
This is a two-way DC/DC converter.24VTO5V5A_1030.pdf