Other Parts Discussed in Thread: BQSTUDIO,
Hi there,
i am trying to perfom a succesful manual learning cycle with a two cell setting. The hardware I am using is the bq40z60EVM-578.
I've calculated the "advanced charge algorithm setting" according to the app-note SLUA750.
I would like to have a fully charged voltage of 8400mV. I am using the charge settings shown below. My problem is that the TC-bit is never(I am using the option when doing the learning cycle) set as the charging process stops too early. ( That's at least what I think. Any suggestion what the problem might be. Wrong calculated values? When is the TC-bit set?
My second question is about the gauge. Even if bqStudio shows 100% charged only 2 LEDs are on. Do I need to perfom a whole learning cycle to get proper indication? I am using two Panasonic NCR18650B cells. Is the Design Capacity (3350mAh, 2412cWh) and design voltage of 7400mV correct?
Thank you very much
Best regards
Thomas