Hello,
As shown in diagram below, what is the maximum voltage we will get at the output? Base voltage is provided by the NOR gate. If the digital circuit is powered by 5V(Internal Regulator). Will the output be clamp at 5-0.6 = 4.3V? The Vcc in our application is 16V. We are targeting to tie Output control to GND and shorting C1, C2 and E1, E2.