Hello
Vin=3.3V, Table2 recommend fco=7.8KHz,my customer select below parameter, so if it is suitable ? how much the range of fco?
R1:130kΩ(±0.1%)
CFF:150pF(±5%)
Fco:8.16kHz(typ)、7.42kHz(min)^8.22kHz(min)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
Vin=3.3V, Table2 recommend fco=7.8KHz,my customer select below parameter, so if it is suitable ? how much the range of fco?
R1:130kΩ(±0.1%)
CFF:150pF(±5%)
Fco:8.16kHz(typ)、7.42kHz(min)^8.22kHz(min)
Hi,
I have notified our expert regarding this topic. Please expect a response by 9/11/19,
Thanks,
Aaron
Hi Fandy,
Your circuit is approx. +/-5% tolerance from 7.8KHz and it is ok to use these values in this circuit.
Kind Regards,
Liaqat