Could you help with your advice for the following questions?
1) Regarding the average current limit feature, it looks TPS63070 has not shutdown with hitting several over current threshold, but something like PWM modulated current limiting which drags down the output voltage, is it correct?
2) If 1) is correct, does the device still work switching until the output voltage drags below 1.2V of short circuit protection level?
3) I'd like to estimate the worst case of the maximum load output current with the figure-20 on the datasheet. I think the figure can’t describe unit variation, but temperature variation only. How much variation we should multiply on it to estimate the worst case?
4) Regarding synchronization to an external clock mode;
4)-1: Is there any problem toggling EN with staying PWM pulse input on the PS/SYNC pin?
4)-2: Do we need some delay time to wait for completing a synchronization? (e.g. XX clocks duration time is required after detected clock from low state)
4)-3: Which is the synchronization dtection trigger rising edge or falling edge?
4)-4: Is there any duty rate limitation on the external synchronization clock input?
Thanks in advance,
S.Sawamoto