hello,
I have two questions.
The QON pin is always open.
(1) Section 9.2.10.1 explains BATFET Disable Mode (Shipping Mode).
Is Shipping Mode when voltage is applied to VBAT when power is not supplied to VBUS and VBAT?
If the answer is Shipping Mode, does that mean that no voltage is output to SYS until the VBUS input is turned on? (Register control is not performed.)
(2) I understand that you can enter Shipping Mode by setting BATFET_DIS bit.
Does the device enter Shipping Mode if both VBUS and VBAT are powered off without setting the BATFET_DIS bit?
best regards